tedkit2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tedkit2

2,865 Views
pavel_kristof
Contributor I

Hello,

I would like to buy tedkit 2. but on NXP site are 2 types: one for 250 second for 250USD, Can you tell me please which is difference?

 

 

 

0 Kudos
Reply
3 Replies

2,851 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @pavel_kristof,

Hope you are doing well.

The OM6716,599 is our Transponder Evaluation and Development Kit 2 base station that supports the LF transponder.

OM 6716/434,599 is the optional RF extension board for RKE/PKE, Supports the 434 MHz UHF frequency band as transmitter and receiver. The OM6716/434 must be added in the housing of the TED-Kit 2 main board (OM6716,599).

Regards,
Eduardo.

0 Kudos
Reply

2,809 Views
pavel_kristof
Contributor I

Thanks for answer,

We need only OM6716,599 (TedKit2) for reading of Hitag AES chip for automotive factory WITTE. Problem is that this kit is not in stock. Please can you confirm that reader chip HTRC110 is sufficient for reading Hitag AESchips? If yes, we will develop our HW for reader. Please exist some library for working with this reader chip? If yes, please tell me for which processor is this library.

Thanks

Pavel Kristof

0 Kudos
Reply

2,789 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I truly apologize, HITAG AES is an automotive product, and it is out of my support scope. I will recommend contacting your distributor (Distributor Network | NXP Semiconductors) for more information on this inquiry.

Regards,
Eduardo.

0 Kudos
Reply