tedkit2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tedkit2

2,811件の閲覧回数
pavel_kristof
Contributor I

Hello,

I would like to buy tedkit 2. but on NXP site are 2 types: one for 250 second for 250USD, Can you tell me please which is difference?

 

 

 

0 件の賞賛
返信
3 返答(返信)

2,797件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @pavel_kristof,

Hope you are doing well.

The OM6716,599 is our Transponder Evaluation and Development Kit 2 base station that supports the LF transponder.

OM 6716/434,599 is the optional RF extension board for RKE/PKE, Supports the 434 MHz UHF frequency band as transmitter and receiver. The OM6716/434 must be added in the housing of the TED-Kit 2 main board (OM6716,599).

Regards,
Eduardo.

0 件の賞賛
返信

2,755件の閲覧回数
pavel_kristof
Contributor I

Thanks for answer,

We need only OM6716,599 (TedKit2) for reading of Hitag AES chip for automotive factory WITTE. Problem is that this kit is not in stock. Please can you confirm that reader chip HTRC110 is sufficient for reading Hitag AESchips? If yes, we will develop our HW for reader. Please exist some library for working with this reader chip? If yes, please tell me for which processor is this library.

Thanks

Pavel Kristof

0 件の賞賛
返信

2,735件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I truly apologize, HITAG AES is an automotive product, and it is out of my support scope. I will recommend contacting your distributor (Distributor Network | NXP Semiconductors) for more information on this inquiry.

Regards,
Eduardo.

0 件の賞賛
返信