sniff mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,054件の閲覧回数
koichimatsuo
NXP Employee
NXP Employee

Our customer, SONY is asking whether MKW30 or MKW40 has implemented sniff mode or not.

Do you plan to implement this mode?

If yes, when will FSL release it ? 

If no, would you tell us the reason? Because we need to tell it to them.

  *H/W does not implement this mode. etc..

Regards,

Koichi

ラベル(1)
0 件の賞賛
返信
1 解決策
3,826件の閲覧回数
mihaidragnea
NXP Employee
NXP Employee

Hello Koichi-san,

According to MKW3x/4x reference manual, the sniff mode is not currently supported by the hardware. The SNF_EN bit from the sniff control register has no effect.

But if your question is about having a BLE/IEEE 802.15.4 sniffer using KW3x/4x the answer is yes, we will have. The planned date is end of Q3 - beginning of Q4 2015.

Regards,

Mihai

元の投稿で解決策を見る

2 返答(返信)
3,827件の閲覧回数
mihaidragnea
NXP Employee
NXP Employee

Hello Koichi-san,

According to MKW3x/4x reference manual, the sniff mode is not currently supported by the hardware. The SNF_EN bit from the sniff control register has no effect.

But if your question is about having a BLE/IEEE 802.15.4 sniffer using KW3x/4x the answer is yes, we will have. The planned date is end of Q3 - beginning of Q4 2015.

Regards,

Mihai

3,826件の閲覧回数
koichimatsuo
NXP Employee
NXP Employee

Hello Mihai_san,

Thank you for your response.

I will inform them of our plan.

Regards,

Koichi

0 件の賞賛
返信