maximum Children

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

maximum Children

3,616件の閲覧回数
baosong_xie
Contributor I

The maximum number of child nodes of the coordinator (router)  to set?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,557件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

The modification should not be done in the .h file, it is needed for you to modify it in the following way.

estephania_mart_0-1609262103236.jpeg

 

Regards, 

Estephania

 

 

3,595件の閲覧回数
baosong_xie
Contributor I

JN5189 zigbee3.0 stack

SDK_2.6.1_JN5189 middleware wireless zigbee

I found that the ZPS_CHILD_TABLE_SIZE parameter in the zps_gen.h file should set the number of child nodes,But the zps_gen.h and zps_gen.c file is a read-only file ,I want to know how to modify the parameters in the file.

For example,Modify the ZPS CHILD TABLE SIZE parameter to the maximum value.

 

0 件の賞賛
返信

3,607件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

Which device are you using ? Also could you please share with me the protocol to be used?

 

Regards,

Estephania

0 件の賞賛
返信

3,593件の閲覧回数
baosong_xie
Contributor I

JN5189 zigbee3.0 stack SDK_2.6.1_JN5189 middleware wireless zigbee I found that the ZPS_CHILD_TABLE_SIZE parameter in the zps_gen.h file should set the number of child nodes,But the zps_gen.h and zps_gen.c file is a read-only file ,I want to know how to modify the parameters in the file. For example,Modify the ZPS CHILD TABLE SIZE parameter to the maximum value

0 件の賞賛
返信