maximum Children

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

maximum Children

3,586 Views
baosong_xie
Contributor I

The maximum number of child nodes of the coordinator (router)  to set?

Labels (1)
0 Kudos
Reply
4 Replies

3,527 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

The modification should not be done in the .h file, it is needed for you to modify it in the following way.

estephania_mart_0-1609262103236.jpeg

 

Regards, 

Estephania

 

 

3,565 Views
baosong_xie
Contributor I

JN5189 zigbee3.0 stack

SDK_2.6.1_JN5189 middleware wireless zigbee

I found that the ZPS_CHILD_TABLE_SIZE parameter in the zps_gen.h file should set the number of child nodes,But the zps_gen.h and zps_gen.c file is a read-only file ,I want to know how to modify the parameters in the file.

For example,Modify the ZPS CHILD TABLE SIZE parameter to the maximum value.

 

0 Kudos
Reply

3,577 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

Which device are you using ? Also could you please share with me the protocol to be used?

 

Regards,

Estephania

0 Kudos
Reply

3,563 Views
baosong_xie
Contributor I

JN5189 zigbee3.0 stack SDK_2.6.1_JN5189 middleware wireless zigbee I found that the ZPS_CHILD_TABLE_SIZE parameter in the zps_gen.h file should set the number of child nodes,But the zps_gen.h and zps_gen.c file is a read-only file ,I want to know how to modify the parameters in the file. For example,Modify the ZPS CHILD TABLE SIZE parameter to the maximum value

0 Kudos
Reply