kw36 phase based ranging issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kw36 phase based ranging issue

2,240件の閲覧回数
Larry3
Contributor I

Hello.

I want to measure BLE carrier signal, then develop phase-based ranging solution on KW36.

Is there any sample application? or Is there any new development board I can use?

Help me plz.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,217件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Larry3 

Could you please help me with more details about your implementation/project?

Our current SDK contains APIs to capture IQ, nonetheless, you will need to develop your own examples with those API's.


The API's can be found at the following path.

              <installation path>\ middleware\wireless\framework_x.y.z\XCVR\MKW36Z

You can find the APIs to capture IQ in the dbg_ram_capture or the dma_capture files.
 

Besides, Would you mind to think about the method of  Localization Based on RSSI Ranging?

If not, you can refer to this AN for details:

KW36 Localization Based on RSSI Ranging Application

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

2,211件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi @Larry3 

Anything else I can do for you on this case?

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信