after disable jn5169 jtag via uart when programe flash , how to open it again?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

after disable jn5169 jtag via uart when programe flash , how to open it again?

2,911 Views
Alex5080
Contributor II

After  disable jn5169 jtag via uart when programe flash,   engneer need update firmware.   how to open jtag interface again to flash hex file?

0 Kudos
Reply
3 Replies

2,834 Views
Alex5080
Contributor II

cannot solve it.  please check attached picture. 

0 Kudos
Reply

2,821 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Based on your screenshot, you are attempting to access an inaccessible device. A possible reason is that the USB cable has been disconnected, or the target device is not in programming mode.

The JN5169 will enter UART programming mode if SPIMISO (DO1) pin 22 is low after RESET.

In our Development Kit, this is handled by the FT232R IC.

 

Best Regards,

Ricardo

0 Kudos
Reply

2,863 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. The JTAG module, that the JN provides, is only for debug purpose.

I would recommend to check the JN51xx Production Flash Programmer, it is a CLI based software tool which allows data and applications to be loaded from a host machine (such as a PC) into the Flash memory associated with an NXP JN51xx wireless microcontroller.

 

Best Regards,

Ricardo

0 Kudos
Reply