Vsen Asen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,292件の閲覧回数
JbaleAlfa
Contributor II

Hi 

 

I have been trying to find out the max voltage ratings of VSEN (Pin 11), ASEN1 and ASEN2 (Pins 11 and 13)

 

Does anyone know what the max voltage ratings of these pins are?

0 件の賞賛
返信
1 解決策
3,263件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below:

diazmarin09_0-1673464128596.png

 

Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).

I hope this information helps.

Regards,

David

元の投稿で解決策を見る

4 返答(返信)
3,264件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below:

diazmarin09_0-1673464128596.png

 

Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).

I hope this information helps.

Regards,

David

3,254件の閲覧回数
JbaleAlfa
Contributor II

thank you David

0 件の賞賛
返信
3,276件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @JbaleAlfa

Hope you are doing well.

Could you please help us with more details about which device you are using?

Regards,
Eduardo.

0 件の賞賛
返信
3,272件の閲覧回数
JbaleAlfa
Contributor II

its the NXQ1TXH5

タグ(1)
0 件の賞賛
返信