Vsen Asen

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vsen Asen

跳至解决方案
3,291 次查看
JbaleAlfa
Contributor II

Hi 

 

I have been trying to find out the max voltage ratings of VSEN (Pin 11), ASEN1 and ASEN2 (Pins 11 and 13)

 

Does anyone know what the max voltage ratings of these pins are?

0 项奖励
回复
1 解答
3,262 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below:

diazmarin09_0-1673464128596.png

 

Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).

I hope this information helps.

Regards,

David

在原帖中查看解决方案

4 回复数
3,263 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below:

diazmarin09_0-1673464128596.png

 

Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).

I hope this information helps.

Regards,

David

3,253 次查看
JbaleAlfa
Contributor II

thank you David

0 项奖励
回复
3,275 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @JbaleAlfa

Hope you are doing well.

Could you please help us with more details about which device you are using?

Regards,
Eduardo.

0 项奖励
回复
3,271 次查看
JbaleAlfa
Contributor II

its the NXQ1TXH5

标记 (1)
0 项奖励
回复