Vsen Asen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vsen Asen

Jump to solution
3,269 Views
JbaleAlfa
Contributor II

Hi 

 

I have been trying to find out the max voltage ratings of VSEN (Pin 11), ASEN1 and ASEN2 (Pins 11 and 13)

 

Does anyone know what the max voltage ratings of these pins are?

0 Kudos
Reply
1 Solution
3,240 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below:

diazmarin09_0-1673464128596.pngdiazmarin09_0-1673464128596.png

 

Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).

I hope this information helps.

Regards,

David

View solution in original post

4 Replies
3,241 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

I hope all is great with you. Thank you for using the NXP communities.

Please review the information below:

diazmarin09_0-1673464128596.pngdiazmarin09_0-1673464128596.png

 

Please note that the nominal operating range is from 0 V to 1.5 V. However, any level between 1.5 V and VDDP has the same effect (as 1.5 V).

I hope this information helps.

Regards,

David

3,231 Views
JbaleAlfa
Contributor II

thank you David

0 Kudos
Reply
3,253 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @JbaleAlfa

Hope you are doing well.

Could you please help us with more details about which device you are using?

Regards,
Eduardo.

0 Kudos
Reply
3,249 Views
JbaleAlfa
Contributor II

its the NXQ1TXH5

Tags (1)
0 Kudos
Reply