Our products use Jn5169,the SDK is JN-SW-4170 v1840 and JN-AN-1218 v1008.
I had configured i2c as salve. The function of APP_vSlaveReceive is called in mainloop. It process the data from master according to the register of SI Slave Masked Interrupt Status(0x02007810)。
The bit of DATA0_WA_MIS in SI Slave Masked Interrupt Status always is set after master send data.Even if the master send a stop signal in i2c bus.Even if the date is read out from data buffer, and the corresponding Interrupt bit is clear.
This issue also cause that the slave can't receive any data from master any more .
Pls help me,thanks.
Hi @Chris_wn,
I hope you are doing great.
What is the initialization of the SI as a slave?
Also, what I the pins that you are using? Do you have a logic analyzer log?
Regards,
Mario