Take the zone of IAS as an example,I can't enroll successfully

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Take the zone of IAS as an example,I can't enroll successfully

1,356件の閲覧回数
leoxie
Contributor I

Hi everyone,

       my english is very poor, please let me know if you have any question. tks.

       when my End-device joined ZHA network, I used vSendEnrollReq(ZONE_ZONE_ENDPOINT); or vSetIASDeviceState(E_IAS_DEV_STATE_READY_TO_ENROLL); but it can't enroll successfully.

c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_start_ZONE.c:151: APP: Switch Power Up
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_start_ZONE.c:154: Test
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:168: APP_vInitialiseNode*eStatusReload=0
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:190: Set Sec state
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:198: ZPS_eAplAfInit
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/Common/Source/haEzJoin.c:182: Default mask saved = 0x07fff800, Mask Set to = 0x00080000
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_zcl_ZONE_task.c:463: eZCL_Status 0
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_zcl_ZONE_task.c:162: Chan Mask 00080000
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_zcl_ZONE_task.c:163:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_zcl_ZONE_task.c:163: RxIdle TRUELoad IAS zone attribute
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/Common/Source/app_ias_save.c:138: eZCL_FindCluster success
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/Common/Source/app_ias_save.c:157: E_IAS_DEV_STATE_JOINED
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/Common/Source/haEzJoin.c:315:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/Common/Source/haEzJoin.c:315: vEZ_Update EZState state 5
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:650: Non Factory New StartE_RUNNING
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:620:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:620: Poll Failed
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_start_ZONE.c:184: OS started
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:302: E_RUNNING
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:321: E_IAS_DEV_STATE_READY_TO_ENROLL
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:323: ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE Event
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:302: E_RUNNING
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:341: MAC_ENUM_SUCCESS or MAC_ENUM_NO_ACK
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:302: E_RUNNING
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:352:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:352: Poll Confirm, No Data
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_sleep_functions.c:233: Check for sleep Enrrolled 0
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_sleep_functions.c:277:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:302: E_RUNNING
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:352:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:352: Poll Confirm, No Data
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_sleep_functions.c:233: Check for sleep Enrrolled 0
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_sleep_functions.c:277:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:302: E_RUNNING
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:352:
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/zha_ZONE_node.c:352: Poll Confirm, No Data
c:/NXP/bstudio_nxp/workspace/JN-AN-1201-ZigBee-Intruder-Alarm-System/ZONE/Source/app_sleep_functions.c:233: Check for sleep Enrrolled 0

0 件の賞賛
返信
1 返信

1,126件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Leo,

Did you try to run the application note? or Can you enroll the device?
Did you see the enroll message in the LCD expansion board?.

Regards,

Mario

0 件の賞賛
返信