Simple Data transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
17,270件の閲覧回数
davidashraf
Contributor V

I am new to Zigbee and I've been trying simple data transfer between two JN5168-001-M00 modules , using Zigbee 3.0 ( JN-SW- 4170 ) and Application Note AN 1229.
The destination get notified correctly when a message arrives , yet I couldn't read the payload successfully.

on the SED node
PDUM_thAPduInstance myInstance =PDUM_hAPduAllocateAPduInstance(apduMyData);
PDUM_u16APduInstanceWriteNBO(myInstance,0,"b",5);
ZPS_teStatus myStatus= ZPS_eAplAfBroadcastDataReq(myInstance,1234,1,255,ZPS_E_BROADCAST_ZC_ZR,ZPS_E_APL_AF_UNSECURE,0,NULL);


on the coordinator endpoint
uint8 u8Payload;
PDUM_u16APduInstanceReadNBO(sStackEvent.uEvent.sApsDataIndEvent.hAPduInst,0,'b',&u8Payload);


whatever the message I try at the SED node , when I check the payload of the coming message it gives 0.

Any one can help ? 
Thanks in advance .

タグ(3)
1 解決策
14,952件の閲覧回数
limcb
Contributor IV

Certainly odd, I just added a ReadNBO (lines 11-14), rebuild SED and broadcast from Coordinator and it works. 

case ZPS_EVENT_APS_DATA_INDICATION:
{
     DBG_vPrintf(TRACE_APP, "APP: APP_taskEndPoint: ZPS_EVENT_AF_DATA_INDICATION\n");

     /* Process incoming cluster messages for this endpoint... */
     DBG_vPrintf(TRACE_APP, "    Data Indication:\r\n");
     DBG_vPrintf(TRACE_APP, "        Profile :%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u16ProfileId);
     DBG_vPrintf(TRACE_APP, "        Cluster :%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u16ClusterId);
     DBG_vPrintf(TRACE_APP, "        EndPoint:%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u8DstEndpoint);

     uint8 u8TempPayload;
     uint16 u16bytesread;
     u16bytesread = PDUM_u16APduInstanceReadNBO(sStackEvent.uEvent.sApsDataIndEvent.hAPduInst,0,"b",&u8TempPayload);
     DBG_vPrintf(TRACE_APP, "Read: %d, Data: %c", u16bytesread, u8TempPayload);

     /* free the application protocol data unit (APDU) once it has been dealt with */
     PDUM_eAPduFreeAPduInstance(sStackEvent.uEvent.sApsDataIndEvent.hAPduInst);
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Do you have any APDU changes to ZBProAppTemplate.zpscfg ?

Clipboard03.png

Edit: I'll try the reverse like your case, SED -> Coordinator. 

Just hardcoded a quick broadcast code to the SED. It works. 

PUBLIC void vWakeCallBack(void)
{
    /* schedule device to go to sleep, then poll for data */
    DBG_vPrintf(TRACE_APP, "APP: Polling for data\n");
    ZPS_eAplZdoPoll();
    
    //
     uint8 u8TransactionSequenceNumber;
    ZPS_tsNwkNib * thisNib;
    thisNib = ZPS_psNwkNibGetHandle(ZPS_pvAplZdoGetNwkHandle());
    PDUM_thAPduInstance hAPduInst;
     hAPduInst = PDUM_hAPduAllocateAPduInstance(apduMyData);

     uint16 u16Offset = 0;
     uint16 i;

     // Fill hAPDU payload
     u16Offset = 0;
     uint8 buffer[] = "idontknow";
     for (i = 0; i < 5; i++) {
          u16Offset += PDUM_u16APduInstanceWriteNBO(hAPduInst, u16Offset,"b", *(buffer + i));
          DBG_vPrintf(TRUE, "%c", *(buffer + i));
     }
     PDUM_eAPduInstanceSetPayloadSize(hAPduInst, u16Offset);
     DBG_vPrintf(TRUE, "Size : %d\nSending : \n", PDUM_u16APduInstanceGetPayloadSize(hAPduInst));


     if (hAPduInst == PDUM_INVALID_HANDLE)
     {
          DBG_vPrintf(TRUE, "PDUM_INVALID_HANDLE\n");
     } else {
          ZPS_teStatus eStatus;
          ZPS_teAplAfSecurityMode  eSecurityMode = (ZPS_E_APL_AF_SECURE_NWK);

          eStatus = ZPS_eAplAfBroadcastDataReq(     hAPduInst,
                                                     0x1337,
                                                     0x01,
                                                     0x01,
                                                     ZPS_E_BROADCAST_ZC_ZR,               //     Dest: All Coordinator & Routers
                                                     eSecurityMode,
                                                     0,
                                                     &u8TransactionSequenceNumber
                                                     );
     }
}

Result from Coordinator,

APP: APP_taskEndPoint: ZPS_EVENT_AF_DATA_INDICATION

Data Indication:

Profile :1234

Cluster :1337

From :4e99

EndPoint:1

Payload Length:5

Payload : idont

元の投稿で解決策を見る

23 返答(返信)
14,434件の閲覧回数
dheerajsawant
Contributor V

Hello davidashraf‌ , mario_castaneda‌, 

i am transmitting data from SED to Coordinator, as per above discussion.

But can you tell me how to get ack from Coordinator because i want reply from coordinator that my Message is delivered or not?

please need your help!

Thank You for your Time!

0 件の賞賛
返信
14,434件の閲覧回数
arthurpulatov
Contributor II

I just need to readout many devices from one using unicast.
Thanks!

0 件の賞賛
返信
14,443件の閲覧回数
arthurpulatov
Contributor II

Hi David! 

Is it possible to send a parcel with Length 255 if change APDU size to 255?

0 件の賞賛
返信
14,434件の閲覧回数
yuboli
Contributor II

Hi  Arthur Pulatov!

How do you configure to send 200 bytes?~HI_N556~GU~G9[(0_&#125;E)17.png

I configure above them, but it is invalid. How to slove it 

Thank!

0 件の賞賛
返信
14,438件の閲覧回数
limcb
Contributor IV

Yes, but you must turn on Fragment and only Unicast. 

Look up Appendix B.1, JN-UG-3113. 

0 件の賞賛
返信
14,443件の閲覧回数
limcb
Contributor IV

Hi, please have a search for 'PDUM_u16APduInstanceWriteNBO' in the file "C:\NXP\bstudio_nxp\sdk\JN-SW-4170\Components\ZCIF\Source\zcl.c" for some usage on that API. 

Try to also set the setsize or setpayloadsize.

0 件の賞賛
返信
14,443件の閲覧回数
davidashraf
Contributor V

Hi , Thanks for your reply 
I've tried this and I don't think the problem is in writing the payload at the sender node
I tried debugging the instance returned on event occurrence at the receiver node and it gives me invalid handle!

This is how I deal with the coming message 

uint8 u8Payload;
PDUM_u16APduInstanceReadNBO(sStackEvent.uEvent.sApsDataIndEvent.hAPduInst,0,'b',&u8Payload);

on trying to print the value of 'u8Payload' it always gives me '0' not matter the actual payload I wrote on the sender node 
and also by trying checking the handle 'sStackEvent.uEvent.sApsDataIndEvent.hAPduInst' it gives invalid handle!

0 件の賞賛
返信
14,443件の閲覧回数
limcb
Contributor IV

Sorry, did not see this part.

The destination get notified correctly when a message arrives , yet I couldn't read the payload successfully.

Please have a look at appZdpExtraction.c under the function zps_bAplZdpUnpackNwkUpdateNotifyResponse.

0 件の賞賛
返信
14,443件の閲覧回数
davidashraf
Contributor V

Can you show me the code you tried at the coordinator for sending , please ?
maybe the problem is in sending as I already tried the same code you used for receiving ,yet still failing to read payload correctly

0 件の賞賛
返信
14,443件の閲覧回数
limcb
Contributor IV

Sending as broadcast or else, you need to access the network table to fetch router's address, etc etc.

Usage:

APP_vSendPayload_Bcast(tempbuf,9,CLUSTER_ID);  

Parameters:

tempbuf = array of bytes,

length = length to send,

CLUSTER ID = get from zps_gen.h

Edit: Oh it sends to endpoint 0x01

PUBLIC void APP_vSendPayload_Bcast(const uint8 *buffer, uint16 length, uint16 clusterID) {
     uint8 u8TransactionSequenceNumber;
    ZPS_tsNwkNib * thisNib;
    thisNib = ZPS_psNwkNibGetHandle(ZPS_pvAplZdoGetNwkHandle());
    PDUM_thAPduInstance hAPduInst;
     hAPduInst = PDUM_hAPduAllocateAPduInstance(apduMyData);

     uint16 u16Offset = 0;
     uint16 i;

     // Fill hAPDU payload
     u16Offset = 0;
     if (length < PDUM_u16APduGetSize(hAPduInst)) {
          for (i = 0; i < length; i++) {
               u16Offset += PDUM_u16APduInstanceWriteNBO(hAPduInst, u16Offset,"b", *(buffer + i));
               DBG_vPrintf(TRACE_TRANSMIT, "%c", *(buffer + i));
          }
          PDUM_eAPduInstanceSetPayloadSize(hAPduInst, u16Offset);
     } else {
          DBG_vPrintf(TRACE_TRANSMIT, "ERR: Payload length exceeded\n");
     }
     DBG_vPrintf(TRACE_TRANSMIT, "Size : %d\nSending : \n", PDUM_u16APduInstanceGetPayloadSize(hAPduInst));


     if (hAPduInst == PDUM_INVALID_HANDLE)
     {
          DBG_vPrintf(TRACE_TRANSMIT, "PDUM_INVALID_HANDLE\n");
     } else {
          ZPS_teStatus eStatus;
          ZPS_teAplAfSecurityMode  eSecurityMode = (ZPS_E_APL_AF_SECURE_NWK);

          eStatus = ZPS_eAplAfBroadcastDataReq(     hAPduInst,
                                                     clusterID,
                                                     0x01,
                                                     0x01,
                                                     ZPS_E_BROADCAST_ZC_ZR,               //     Dest: All Coordinator & Routers
                                                     eSecurityMode,
                                                     0,
                                                     &u8TransactionSequenceNumber
                                                     );
     }
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍
0 件の賞賛
返信
14,443件の閲覧回数
davidashraf
Contributor V

I tried that but
when I debug as follows at the receiving node 

if (sStackEvent.uEvent.sApsDataIndEvent.hAPduInst==PDUM_INVALID_HANDLE)
{
DBG_vPrintf(TRACE_APP, "Invalid Handle \n");
}else{
DBG_vPrintf(TRACE_APP, "Valid Handle\n");
}

It gives " Invalid Handle "!

Also when trying to read the payload :

u16BytesRead=PDUM_u16APduInstanceReadNBO(sStackEvent.uEvent.sApsDataIndEvent.hAPduInst,u16PayloadPos,"b",&u8Payload);
DBG_vPrintf(TRACE_APP, "        PayloadSize:%x\r\n",u16BytesRead);

It gives 0!


0 件の賞賛
返信
14,443件の閲覧回数
limcb
Contributor IV

You need to call your ReadNBO routine at :

vHandleStackEvent in app_router or

APP_vtaskMyEndPoint in app_endpoint

It gets cleared as soon as it exits the function vHandleStackEvent or APP_vtaskMyEndPoint. 

The stack processes the Event only once then forgets all about it as soon as it leaves the 2 function above. 

You may not declare ZPS_tsAfEvent sStackEvent; anywhere in the program and ReadNBO it. 

( at least I think what is happening here )

0 件の賞賛
返信
14,443件の閲覧回数
davidashraf
Contributor V

I am trying to send from a SED to the coordinato
I call ReadNBO at : APP_vtaskMyEndPoint in app_endpoint 

The strange thing is that the message arrives and get collected 
and by debugging :
DBG_vPrintf(TRACE_APP, " Profile :%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u16ProfileId);
DBG_vPrintf(TRACE_APP, " Cluster :%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u16ClusterId);
DBG_vPrintf(TRACE_APP, " EndPoint:%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u8DstEndpoint);t doesn't make any sens

it gives the right data  ( profile ID , cluster ID , Dest End point ) 

only it fails to read the payload and finds the apdu instance invalid!! 

14,953件の閲覧回数
limcb
Contributor IV

Certainly odd, I just added a ReadNBO (lines 11-14), rebuild SED and broadcast from Coordinator and it works. 

case ZPS_EVENT_APS_DATA_INDICATION:
{
     DBG_vPrintf(TRACE_APP, "APP: APP_taskEndPoint: ZPS_EVENT_AF_DATA_INDICATION\n");

     /* Process incoming cluster messages for this endpoint... */
     DBG_vPrintf(TRACE_APP, "    Data Indication:\r\n");
     DBG_vPrintf(TRACE_APP, "        Profile :%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u16ProfileId);
     DBG_vPrintf(TRACE_APP, "        Cluster :%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u16ClusterId);
     DBG_vPrintf(TRACE_APP, "        EndPoint:%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u8DstEndpoint);

     uint8 u8TempPayload;
     uint16 u16bytesread;
     u16bytesread = PDUM_u16APduInstanceReadNBO(sStackEvent.uEvent.sApsDataIndEvent.hAPduInst,0,"b",&u8TempPayload);
     DBG_vPrintf(TRACE_APP, "Read: %d, Data: %c", u16bytesread, u8TempPayload);

     /* free the application protocol data unit (APDU) once it has been dealt with */
     PDUM_eAPduFreeAPduInstance(sStackEvent.uEvent.sApsDataIndEvent.hAPduInst);
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Do you have any APDU changes to ZBProAppTemplate.zpscfg ?

Clipboard03.png

Edit: I'll try the reverse like your case, SED -> Coordinator. 

Just hardcoded a quick broadcast code to the SED. It works. 

PUBLIC void vWakeCallBack(void)
{
    /* schedule device to go to sleep, then poll for data */
    DBG_vPrintf(TRACE_APP, "APP: Polling for data\n");
    ZPS_eAplZdoPoll();
    
    //
     uint8 u8TransactionSequenceNumber;
    ZPS_tsNwkNib * thisNib;
    thisNib = ZPS_psNwkNibGetHandle(ZPS_pvAplZdoGetNwkHandle());
    PDUM_thAPduInstance hAPduInst;
     hAPduInst = PDUM_hAPduAllocateAPduInstance(apduMyData);

     uint16 u16Offset = 0;
     uint16 i;

     // Fill hAPDU payload
     u16Offset = 0;
     uint8 buffer[] = "idontknow";
     for (i = 0; i < 5; i++) {
          u16Offset += PDUM_u16APduInstanceWriteNBO(hAPduInst, u16Offset,"b", *(buffer + i));
          DBG_vPrintf(TRUE, "%c", *(buffer + i));
     }
     PDUM_eAPduInstanceSetPayloadSize(hAPduInst, u16Offset);
     DBG_vPrintf(TRUE, "Size : %d\nSending : \n", PDUM_u16APduInstanceGetPayloadSize(hAPduInst));


     if (hAPduInst == PDUM_INVALID_HANDLE)
     {
          DBG_vPrintf(TRUE, "PDUM_INVALID_HANDLE\n");
     } else {
          ZPS_teStatus eStatus;
          ZPS_teAplAfSecurityMode  eSecurityMode = (ZPS_E_APL_AF_SECURE_NWK);

          eStatus = ZPS_eAplAfBroadcastDataReq(     hAPduInst,
                                                     0x1337,
                                                     0x01,
                                                     0x01,
                                                     ZPS_E_BROADCAST_ZC_ZR,               //     Dest: All Coordinator & Routers
                                                     eSecurityMode,
                                                     0,
                                                     &u8TransactionSequenceNumber
                                                     );
     }
}

Result from Coordinator,

APP: APP_taskEndPoint: ZPS_EVENT_AF_DATA_INDICATION

Data Indication:

Profile :1234

Cluster :1337

From :4e99

EndPoint:1

Payload Length:5

Payload : idont

14,443件の閲覧回数
dheerajsawant
Contributor V

Hello Lim, 

I was little bit confuse about this data transfer between SED to Co-ordinator. 

but after so many try and error it become successful :smileyhappy: to data transfer between SED to CO-Ordinator. 

But, 

Now i am trying to send data from Co-Ordinator to SED and i don't know how to start from co-ordinator. 

need your help. 

Thank You for Your Time!

0 件の賞賛
返信
14,443件の閲覧回数
dheerajsawant
Contributor V

Hello Sir, 

I am doing the same thing but its showing me error 

!!! Alignment error

i check the code this error comes after 

thisNib = ZPS_psNwkNibGetHandle(ZPS_pvAplZdoGetNwkHandle());
i read thisNib Value its show
thisNib Read :  4001944
i think problem is in this line--> hAPduInst = PDUM_hAPduAllocateAPduInstance(apduMyData);
After that i saw below message
!!! Alignment error
u32PICMR = 0 : u32PICSR = 8
u32PICMSR = 0 : u32IPMR = 4
u32IHPR = 7 : u32AINT = 8 u32PINT 0
EPCR = 8840b : EEAR = deadbf55
 then long values comes continuously 
  4007a18 : 0000000c
 4007a1c : 0008840b
 4007a20 : deadbf55
 4007a24 : 00000000
 4007a28 : 00000007
 4007a2c : 00000004
 4007a30 : 00000008
 4007a34 : 00000000
 4007a38 : 00000000
Like this and
after that my 
device reset by watchdog timer 

APP: Power Up
APP: Watchdog timer has reset device!
:smileysad: too bad for me. 
can i get your help.
 Please need your help!

Thank you for your Time!

0 件の賞賛
返信
14,443件の閲覧回数
terrysi
Contributor I

Hi,Lim.I use this code to send and read data in the 1184 demo project. But when try to continuouos send data,everything seems ok with the first tow datas, but the coordinator can't receive any data after that while the debug message from the enddevice show show the data is sent successfully.And when enddevice sends the 8th data, the debug message began to show "No free MCPS request descriptor" error. Has you ever encountered this problem?

0 件の賞賛
返信
14,443件の閲覧回数
davidashraf
Contributor V

It finally worked! 
Thank you very much for your time :smileyhappy:

0 件の賞賛
返信
14,443件の閲覧回数
dheerajsawant
Contributor V

Hello Sir, 

I am working on ZigBeePro Stack. I have install ZPS Editor. 

and set parameter as per JN-UG-3113 PDF. 

i create APDU by name "TestApdu" in Sleeping Endevice. 

i have added screen shot so you will understand better. 

apdu_call.png

TestApdu.png

how to remove that error?

please suggest me something. 

i am really stuck on it. 

Thank You For Your Reply.

0 件の賞賛
返信
14,443件の閲覧回数
davidashraf
Contributor V

I am still having the problem 
The message reaches the destination but when I check for the apdu instance it turns out to be invalid! 
Is there something wrong in my code or what ? 

0 件の賞賛
返信