Queries about KW-45s Demo Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Queries about KW-45s Demo Application

820 Views
parvez2001
Contributor I

I am using KW-45 BLE EVK with NCJ29D6 for their SPI communication demo application (kw45b41zevk_digital_key_device_freertos). In which the KW-45  being SPI Host sending Get_FW_Version UCI command to NCJ29D6 and NCJ29D6 is sending response to this command. my question is "Can i send other UCI commands like Set_app_configuration, Start_Ranging / Stop_Ranging etc from KW045 to NCJ29D6 without making any changes in NCJ29D6's Testware Application? And if this is possible then can i do it with another pair of KW-45 and NCJ29D6 make Two NCJ29D6 have UWB Ranging making one as an initiator and another one as a responder." 

If this is not possible, please help me with some suggestions regarding the same.

Thanks and regards.

0 Kudos
Reply
1 Reply

802 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Sorry for the inconvenience this might cause you, but as the question is more related to the NCJ29D6, and the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public, this is not a secure channel to share any information of this device, and I do not have the data as well for the same reason.

For more information about the chip could you please contact one of our distributors available in the Distributor Network|NXP? Or if you have a direct contact who helped you with information about this product in a first place, please communicate with him/her.

 

Regards,

Ricardo

0 Kudos
Reply