QN9090-DK006 example code & UUID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9090-DK006 example code & UUID

ソリューションへジャンプ
2,117件の閲覧回数
TM33
Contributor I

I'm trying to send and receive data over Bluetooth using QN9090-DK006.
Create numbers with QN9090-DK006 and check the data on the PC side via Bluetooth.
The sdk I am currently referring to is qn9090dk6_hid_device_bm.
This is automatically recognized as Mouse on the PC.
I want it to be recognized as Device instead of Mouse.
I want to change the UUID setting, but I don't know where it is described.

Is it okay to use the sdk qn9090dk6_hid_device_bm as a reference for the function I want to achieve?
Please let me know if there is a better sdk sample.
I would like to know the file and value set for UUID in sdk.

0 件の賞賛
返信
1 解決策
2,096件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @TM33 ,

 

Thanks for contacting NXP support.

NXP provides a rich set of sample projects to help with BLE development. If you want to send and receive data over Bluetooth using QN9090-DK006, we believe that Wireless UART is a better DEMO for your requirements. 

The application is built to work with another supported platform running the same example or with the Wireless UART from the IoT Toolbox application. With this sample project, you can try to implement data transfer between two QN9090 boards or one board and mobile app.

For more detailed implementation and usage instructions, as well as for other examples in the SDK, please refer to this document: Bluetooth Low Energy Demo Applications User's Guide.pdf ,  which located at this path: SDK_Root_Path\docs\wireless\Bluetooth\Bluetooth Low Energy Demo Applications User's Guide.pdf

Hope you are doing well!

 

Best regards,

Gavin

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,097件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @TM33 ,

 

Thanks for contacting NXP support.

NXP provides a rich set of sample projects to help with BLE development. If you want to send and receive data over Bluetooth using QN9090-DK006, we believe that Wireless UART is a better DEMO for your requirements. 

The application is built to work with another supported platform running the same example or with the Wireless UART from the IoT Toolbox application. With this sample project, you can try to implement data transfer between two QN9090 boards or one board and mobile app.

For more detailed implementation and usage instructions, as well as for other examples in the SDK, please refer to this document: Bluetooth Low Energy Demo Applications User's Guide.pdf ,  which located at this path: SDK_Root_Path\docs\wireless\Bluetooth\Bluetooth Low Energy Demo Applications User's Guide.pdf

Hope you are doing well!

 

Best regards,

Gavin

0 件の賞賛
返信