QN9080SIP BLE Address and Royalties

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

QN9080SIP BLE Address and Royalties

跳至解决方案
2,973 次查看
davideferrario
Contributor II

I am starting a project based on QN9080SIP.

I am afraid about two topics:

- the QN9080SIP module comes with programmed unique BLE MAC address?

- what about BLE royalties? Should they be paid or are they included in QN9080SIP cost?

Thank you

0 项奖励
回复
1 解答
2,966 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Every board has different MAC address. It won't be repeated. You needn't pay for it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,962 次查看
Xiang_Li
NXP Employee
NXP Employee

For the BLE royalties, you need to check the Bluetooth SIG product qualification & listing procedures.

NXP has done most part of BLE testings when qualify QN9080. But the final product based on QN9080 should be still qualified once, under the vendor company of the end product.

 

0 项奖励
回复
2,967 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Every board has different MAC address. It won't be repeated. You needn't pay for it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复