QN9080SIP BLE Address and Royalties

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9080SIP BLE Address and Royalties

Jump to solution
2,953 Views
davideferrario
Contributor II

I am starting a project based on QN9080SIP.

I am afraid about two topics:

- the QN9080SIP module comes with programmed unique BLE MAC address?

- what about BLE royalties? Should they be paid or are they included in QN9080SIP cost?

Thank you

0 Kudos
Reply
1 Solution
2,946 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Every board has different MAC address. It won't be repeated. You needn't pay for it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,942 Views
Xiang_Li
NXP Employee
NXP Employee

For the BLE royalties, you need to check the Bluetooth SIG product qualification & listing procedures.

NXP has done most part of BLE testings when qualify QN9080. But the final product based on QN9080 should be still qualified once, under the vendor company of the end product.

 

0 Kudos
Reply
2,947 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Every board has different MAC address. It won't be repeated. You needn't pay for it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply