QN9080SIP BLE Address and Royalties

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9080SIP BLE Address and Royalties

ソリューションへジャンプ
2,968件の閲覧回数
davideferrario
Contributor II

I am starting a project based on QN9080SIP.

I am afraid about two topics:

- the QN9080SIP module comes with programmed unique BLE MAC address?

- what about BLE royalties? Should they be paid or are they included in QN9080SIP cost?

Thank you

0 件の賞賛
返信
1 解決策
2,961件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Every board has different MAC address. It won't be repeated. You needn't pay for it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,957件の閲覧回数
Xiang_Li
NXP Employee
NXP Employee

For the BLE royalties, you need to check the Bluetooth SIG product qualification & listing procedures.

NXP has done most part of BLE testings when qualify QN9080. But the final product based on QN9080 should be still qualified once, under the vendor company of the end product.

 

0 件の賞賛
返信
2,962件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Every board has different MAC address. It won't be repeated. You needn't pay for it.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信