QN9080 BLE overflow problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9080 BLE overflow problem

1,798 Views
tpgurtpgur2
Contributor I

Hi, I'm trying to solve the BLE overflow problem.

My project is to send data from client custom device using QN9080-M17 to QN9080-DK.

The problem is that after a certain time, an overflow error appears and no data is sent.

We use wireless_uart example form SDK_2.x_QN908XCDK and we send data using battery measurement timer callback function.

Our time interval is 20ms and we send data length of 60 bytes at same interval.

I checked the "gBleOverflow_c" error is the return value of BLE API functions...so I cannot solve this problem.

How can I solve this problem?

0 Kudos
Reply
1 Reply

1,654 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

The API adds to the queue in the controller, if it returns a gBleOverflow_c it means that the queue it's full and you need to wait until you can send a new message, I'll need to investigate further on this.

By any chance, did you modify something else? When you mention a custom device, are you referring to custom profile or are you referring to a custom board ?

And just to confirm, in your test it starts working correctly and sending the data and after some time it stops? Or It never sends the data ?

Regards,

Estephania

0 Kudos
Reply