QN9020 Simultaneous Peripheral and Observer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9020 Simultaneous Peripheral and Observer

ソリューションへジャンプ
2,391件の閲覧回数
mikebwilliams
Contributor II

I have a device that is a simple peripheral that will support a few basic profiles. However, I also need this device to receive broadcast advertisements from other devices at the same time. I effectively want it to always pass advertisement packets up to my code regardless of any other state it's in. Can the QN902X do this? 

タグ(1)
0 件の賞賛
返信
1 解決策
2,254件の閲覧回数
mikebwilliams
Contributor II

NXP has confirmed this functionality does not work.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,254件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Mike,

While the QN9020 is in the Central role the QN9020 shall support eight connections at the same time. Otherwise, only one.

Best Regards,

Mario

0 件の賞賛
返信
2,255件の閲覧回数
mikebwilliams
Contributor II

NXP has confirmed this functionality does not work.

0 件の賞賛
返信