Whats the deal with ZigBee and Thread Stack Compilers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whats the deal with ZigBee and Thread Stack Compilers

1,730 Views
tgsoverly
Contributor I

I have been trying to understand the NXP website for sometime, and mostly failing.

I am trying to evaluate various platforms out there to do some ZigBee and hopefully Thread development.  

My requirements:

  1. I work on Macs, so IAR compilers aren't really an option, especially for just trying some low volume prototyping at this point.
  2. The platform must have ZigBee
  3. I would really like it to have Thread

What I "think" is up with NXP

  1. They have the KW2x line that has a Thread/BLE/802.15.4 for GCC compilers, but the BeeStack must us IAR.
  2. The have the JN517x line that has a ZigBee 3.0 Stack for GCC but no plans for Thread.

Actual questions:

  1. Any of what I "think" correct?
  2. Anyone have any clue if they going to support ZigBee on the KW2x, or Thread on the JN517x?

I am really sorry if this is the wrong place or has been answered some place else, and thank you very much for you time.  This stuff is so much harder than actually making stuff.

Cheers!

1 Reply

1,593 Views
jc_pacheco
NXP Employee
NXP Employee

Hello Tim, 

There are plans to add ZigBee 3.0 support for KW41Z in Q3 2017. This includes GCC and IAR compilers.