PN7150

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
4,390 次查看
sjvg
Contributor I

Hi,

What is the preferred differential trace impedance for TX output and RX Input for PN7150 NFC IC?Can we consider it as 100 Ohms?

Regards

0 项奖励
回复
1 解答
4,385 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Differential trace has no requirements for impedance because it is not a high-frequency line.

Hope it help you.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,386 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Differential trace has no requirements for impedance because it is not a high-frequency line.

Hope it help you.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 项奖励
回复
4,378 次查看
sjvg
Contributor I

Hi Fangfang

Thank you.

 

0 项奖励
回复