PN7150

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,383件の閲覧回数
sjvg
Contributor I

Hi,

What is the preferred differential trace impedance for TX output and RX Input for PN7150 NFC IC?Can we consider it as 100 Ohms?

Regards

0 件の賞賛
返信
1 解決策
4,378件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Differential trace has no requirements for impedance because it is not a high-frequency line.

Hope it help you.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,379件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Differential trace has no requirements for impedance because it is not a high-frequency line.

Hope it help you.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 件の賞賛
返信
4,371件の閲覧回数
sjvg
Contributor I

Hi Fangfang

Thank you.

 

0 件の賞賛
返信