PN7150 Maximum Output Power

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7150 Maximum Output Power

1,268件の閲覧回数
gwctree42
Contributor I

I have a NFC reader application based on PN7150, currently powered with VBAT=VBAT1=VBAT2=3.3V
Is the only way to increase output power to increase the VBAT voltage or is there some output Tx setting I could check? 

Is the highest possible output Tx power VBAT=VBAT1=VBAT2=5V, and then update the PMU_CFG register to specify VBAT1=5V and TxLDO = 4.7V ?

0 件の賞賛
返信
1 返信

1,253件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @gwctree42

Hope you are doing well.

Please, consider that PN7150 device is not recommended for new designs. We recommend using the PN7160 instead.

TXLDO has the possibility to generate 4.75 V or 4.5 V to supply the transmitter with the regulator being supplied by external 5V. Typical current load should be up to 180mA.

More information on this can be found in UM10936, Section 5.7.2 CFG2 Transmitter supply voltage from external 5V supply; and PN7150 Data Sheet, Section 12.5.3 TXLDO.

Regards,
Eduardo.

0 件の賞賛
返信