OTA Bootloader Example for MCXW71

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTA Bootloader Example for MCXW71

ソリューションへジャンプ
1,543件の閲覧回数
VeridianJack
Contributor III

Reading through the Bluetooth® Low Energy Application Developer’s Guide.

There should be an example project that implements OTA BLE through a bootloader.

The OTAP Bootloader project and source code can be found in the \boards\<board>\wireless_examples\framework\bootloader_otap\ folder.

 

Does this example exist for the MCXW71 / KW45 chips?

Which SDK would have this example that could be most easily ported?

0 件の賞賛
返信
1 解決策
1,523件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello

 

To use the OTAP Bootloader I would recommend using the KW45B41Z-EVK SDK Most Recent Version (25.03.00), the example you'll need to implement is the [otap_client_att_freertos]

 

I would recommend checking the Bluetooth Low Energy Demo Applications User’s Guide Chapter 5.11 for further information about OTAP in KW45. Bluetooth Low Energy Demo Applications User’s Guide

 

Also, This Application note can be useful regarding the KW45 OTAP bootloader Creating Firmware Update Image for KW45B41Z/K32W148 using Over the Air Programming Tool

 

Best Regards

Luis

元の投稿で解決策を見る

1 返信
1,524件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello

 

To use the OTAP Bootloader I would recommend using the KW45B41Z-EVK SDK Most Recent Version (25.03.00), the example you'll need to implement is the [otap_client_att_freertos]

 

I would recommend checking the Bluetooth Low Energy Demo Applications User’s Guide Chapter 5.11 for further information about OTAP in KW45. Bluetooth Low Energy Demo Applications User’s Guide

 

Also, This Application note can be useful regarding the KW45 OTAP bootloader Creating Firmware Update Image for KW45B41Z/K32W148 using Over the Air Programming Tool

 

Best Regards

Luis