BLE BD address generation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE BD address generation

2,480件の閲覧回数
pangya
Contributor I

The BD address is generated according to the radio RADIO_CTRL->UID_LSB and random numbers, but why do I access the RADIO_CTRL->UID_LSB register with 0xff, what is the IFR address mapped by this register? Is the UID provided by the chip factory?

0 件の賞賛
返信
6 返答(返信)

2,446件の閲覧回数
pangya
Contributor I

Hello 

1.KW45B41
2.adv_ext_peripheral,   SDK_24_12_00_KW45B41Z-EVK.
Does the K45 chip currently have a public SIG-assigned address? I need each device's BD_ADDR to be immutable. Alternatively, can a unique and permanent BD_ADDR be generated from the chip's unique ID?

0 件の賞賛
返信

2,396件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee
Hello

The KW45B41 is the EVK, LOC or a Custom Board? I need to confirm this as NXP boards have some configuration predetermined.
0 件の賞賛
返信

2,330件の閲覧回数
pangya
Contributor I

Hello

EVK

0 件の賞賛
返信

2,306件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello

The SDK uses a public device address by default and has a fixed OUI

I would recommend checking this application note as I believe it might solve your doubts regarding BD Address

Chapter 2 - Why do we need random static device address

AN14645: How to Use Random Static Device Address for Bluetooth Application | NXP Semiconductors

 

Best Regards

Luis

0 件の賞賛
返信

2,458件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello

 

Could you help us confirm the following question to have more context, please:

What NXP chip are you using?

What example are you using? What SDK version are you using?

 

Best Regards

Luis

0 件の賞賛
返信

2,417件の閲覧回数
pangya
Contributor I

Hello

      Are there any updates on the issue?

Best Regards

pangya

 

 

0 件の賞賛
返信