Not able to compile KW41Z example code with latest SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to compile KW41Z example code with latest SDK

1,927件の閲覧回数
vishnubeema
Contributor III

Hello,

 

I am facing issues with latest KW41Z SDK. Please let me know your inputs. I was going through below link for installation.

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-c...

 I am facing issues in compiling example code. Below are my queries and steps followed.

 

1. As per video IDE is of version “MCUXpressoIDE_0.0_344.exe”. But when I download, it is of “MCUXpressoIDE_10.1.0_589.exe” version.

2. In “3. Build, Run” tab, as part of building, below is snapshot from Video.

 1.jpg

 

But in my tool it is shown as below. I changed to UART. Are these settings are fine ??

I am using ieee_802_15_4 -> mwa_coordinator (with freertos option).

 2.jpg

 

3. I unchecked “Include semihost HardFault handler”. Is this fine ??

 3.jpg 

Whereas in video this option is not present.

4.jpg

 

4. If I build, I am getting compiler errors.

 5.jpg

 

5. I am not sure why these errors are coming (In few cases, include files are not included. These include files are under compile time macros. But why these macros are enabled by default). Even if I change compiler, from “Compiler default” to “-std=gnu99” still I am getting same errors. Are there any settings to be changed in latest IDE so that macros are enabled ??

6.jpg

Thanks & Regards

Vishnu Beema

0 件の賞賛
返信
2 返答(返信)

1,727件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

This is a duplicate question of Not able to compile KW41Z example code with latest SDK.

For your future questions please only post them one time on the corresponding space.

Best regards,

Gerardo

0 件の賞賛
返信

1,727件の閲覧回数
vishnubeema
Contributor III

Hello Gerardo,

I am new to this form.

Initially I added in "Discussion". Later I realized and added in "Ask a Question".

But I could not delete my query from "Discussion" form. Can you please let me know if there is any such feature.

Thanks & Regards

Vishnu Beema

0 件の賞賛
返信