Node cannot access the network after power failure and reconnection (transmission distance becomes shorter)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Node cannot access the network after power failure and reconnection (transmission distance becomes shorter)

5,625件の閲覧回数
jun951753jun951
Contributor III

I use 1229

Connect power after power off, the node can not enter the network。

Only when the node is very close to the coordinator can it enter the network again (5m)

ラベル(3)
6 返答(返信)

5,474件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

The JN-AN-1229 is not saving the Zigbee network, so if you restart the device it will start as factory reset.

Regards,

Mario

5,474件の閲覧回数
jun951753jun951
Contributor III

我使用jn 5168-001-m03和1229模式。

我使用路由器收集和上传数据,数据传输在工作中是正常的,但传输距离太近(10米),我找不出原因,请帮我看看问题出在哪里。

0 件の賞賛
返信

5,474件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

Is it possible that you could share your question in English?

What is the channel that you are working on? I am assuming that you have the JN module, do you have any interference arround?

Regards,

Mario

0 件の賞賛
返信

5,474件の閲覧回数
jun951753jun951
Contributor III

This is my code

0 件の賞賛
返信

5,474件の閲覧回数
jun951753jun951
Contributor III

I use 5168-m03 and 1229.I tested it indoors without any interference.

I use the router to collect and upload data, and the data transmission is normal in work, but the transmission distance is too close (10 meters), I can't find out the reason, please help me to see what the problem is.

0 件の賞賛
返信

5,473件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi, 

Could you please try to use the Channel 25 for example?

Please look at the file attached.

Regards,

Mario

0 件の賞賛
返信