Network key disabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,300件の閲覧回数
jasonchiang
NXP Employee
NXP Employee

Hi,

  Under Beekit configuration, there is network key setup. If the value is set all 00s, the trust center will generate a random network key.

How to disable this network key setup ? As I would like to see ASDU data without any security. What kind of security key used in current default images under Zed1.6.5/Embedded/KW24D512TwrHa/


0 件の賞賛
返信
1 解決策
3,102件の閲覧回数
AngelC
Senior Contributor I

Dear Tzyy-Hong,

If you would like to modify the security settings of the images used in ZeD 1.6.5 you should first open the corresponding BeeKit solution file located in folder: C:\Program Files (x86)\Freescale\ZeD 1.6.5\BeeKitSolutionFiles.

In this case it would be the ZigBeeHcApps_TWR_KW24D512_CB401.bksln or, ZigBeeHcApps_TWR_KW24D512_CB400.bksln depending in the codebase you have in BeeKit. Once open, you may see all of the projects in the right side under “Project explorer”, see image below:

Capture5.PNG.png

There you may click on “BeeStack” and change the stack profile to “No security with mesh routing – Stack Profile 2”.

IMPORTANT: Use this only for testing purposes. Real ZHA application may require security settings.

Regards,

AngelC

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,103件の閲覧回数
AngelC
Senior Contributor I

Dear Tzyy-Hong,

If you would like to modify the security settings of the images used in ZeD 1.6.5 you should first open the corresponding BeeKit solution file located in folder: C:\Program Files (x86)\Freescale\ZeD 1.6.5\BeeKitSolutionFiles.

In this case it would be the ZigBeeHcApps_TWR_KW24D512_CB401.bksln or, ZigBeeHcApps_TWR_KW24D512_CB400.bksln depending in the codebase you have in BeeKit. Once open, you may see all of the projects in the right side under “Project explorer”, see image below:

Capture5.PNG.png

There you may click on “BeeStack” and change the stack profile to “No security with mesh routing – Stack Profile 2”.

IMPORTANT: Use this only for testing purposes. Real ZHA application may require security settings.

Regards,

AngelC

0 件の賞賛
返信