Module with SN5169 or SN5179, 125 °C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Module with SN5169 or SN5179, 125 °C

1,488 次查看
juergen_schwage
Contributor I

SN5169 or SN5179

I would like to test a module with integrated antenna in an environment with 125 °C. All the modules I found are only specified up to 85 °C. Is it possible to order an amount of modules with the 125-degree-IC on it?

标签 (1)
  • JN

0 项奖励
回复
3 回复数

1,413 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Juergen,

Just to confirm, is the JN5169 that you are referring for? 

The JN5169 Module Temperature range: 40 C to +85 C.

Unfortunately, we do not provide a module that supports 125 C

Regards,

Mario

0 项奖励
回复

1,413 次查看
juergen_schwage
Contributor I

Thank you for this information.
Sorry for my typing error: This question concerns the ICs JN5169 and JN5179.

Which is the best way to realise a board with one of these ICs? From the customers point of view, I think the best way is to take the NXP-Designs for modules with integrated antenne, produce a PCB, and populate it with the 125-degree-version of the SoC. Does NXP provide the schematics and PCB-Designs of the modules to customers?

0 项奖励
回复

1,413 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Juergen,

I recommend the JN5169 device, the IC supports 125 grades, but the JN516X module supports 85-degree.

 Does NXP provide the schematics and PCB-Designs of the modules to customers?

Support Resources for JN516x MCUs

JN-RD-6038 and the JN-RD-6036

Regards,

Mario

0 项奖励
回复