Looking for SPI command data for in-circuit programming JN5168 on HP3070

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for SPI command data for in-circuit programming JN5168 on HP3070

1,706件の閲覧回数
timstinchcombe
Contributor I

We are migrating our boards from JN5148 to JN5168 modules.

Currently we use the SPI bus to program the M25P10 EEPROM chip inside the JN5148 using our Agilent HP3070 in-circuit testers during the production test of the boards. In the JN5168 the memory is taken inside the main chip in the module, and so we seek details of the commands to program/read memory, read status registers etc. to enable us edit the existing program to talk to the newer JN5168 module.

So far my searching of the usual documentation online hasn't yielded the required data, though I assume it must exist somewhere! Any help much appreciated!

Tim

0 件の賞賛
返信
1 返信

1,537件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Tim

Yes, we do have a user guide JN-UG-3087 which explains about SPI interface commands as well as Flash memory functions to read , program and erase flash in JN516x devices.

 

The commands for the status registers for JN516x are not avialble.

Best Regards,

Mario

0 件の賞賛
返信