Kinetis Pin Compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Pin Compatibility

ソリューションへジャンプ
3,358件の閲覧回数
atillametetured
Contributor V

Hello,

I am at the edge of selecting our ZigBee and Thread Device and am torn between MKW21D512, MKW22D512 and MKW24D512. Are these devices pin compatible. What I think is MKW21D512 is not compatible with 22D and 24D. Can someone confirm this? Also all devices share the same memory properties so I assume they all support ZigBee and Thread simultaneously (I know only 24D supports SE 2.0 profile, I dont know the reason though, can someone also point out why?)

Thanks in advance for help,

Best Regards,

Mete

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
3,048件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Mete,

As you can see MKW2xD Reference Manual​, these three devices have differences only in the Smart Energy, USB and FlexMemory support.

MKW2XD.jpg

Best regards,

Earl Ramírez.

元の投稿で解決策を見る

1 返信
3,049件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Mete,

As you can see MKW2xD Reference Manual​, these three devices have differences only in the Smart Energy, USB and FlexMemory support.

MKW2XD.jpg

Best regards,

Earl Ramírez.