KW45 gpio injection current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 gpio injection current

3,249 Views
Lingyinglu
Contributor I

Hi Guys

Here is a quetion for the KW45 gpio injection current.I want to know why the KW45 injection current

is limit to zero.I've used the othe chipset like KW35/36/38, and I've never seen its injectioncurrent is zero.

I ues one ADC PIN of KW45 to detect the input voltage of Automotive Battery,the Volatage may exceed 3.3v+0.3v=3.6V,this will cause the injection current >0mA.Is any suggestion?

KW45datasheetREV.9.datasheet "page13"

Lingyinglu_0-1689058003907.png

 

0 Kudos
Reply
2 Replies

2,842 Views
ChristianSchweer
Contributor II

Hello @Gavin_Jia ,

Unfortunately, the answer about the injection current is not enough for me. The KW45 data sheet clearly states that no injection current is permitted. Even if a resistor is used, there will always be an injection current through the clampling diodes.

ChristianSchweer_0-1725018049765.png

 

Can you please tell me the relevant passages in the KW45 that confirm safe operation despite the injection current.

Thanks in advance,

Christian

Tags (1)
0 Kudos
Reply

3,224 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Lingyinglu ,

 

Thanks for contacting NXP support.

Judging from this datasheet, if the I/O pins can observe the limit, then is no need to provide current limiting resistors at the pads, otherwise current limiting resistors is needed. For details on how to select the current limiting resistor and injection current, you can refer to this AN: AN4731 Understanding Injection Current on NXP Automotive Microcontrollers

 

Best regards,

Gavin

0 Kudos
Reply