Compatibility of RC523 with MUAES Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatibility of RC523 with MUAES Card

1,076件の閲覧回数
jf555
Contributor I

Hello everyone,

I'm currently working on a project that involves using NXP's RC523 RFID reader chip. I plan to use it in conjunction with MUAES (MIFARE Ultralight AES) cards, but I'm uncertain about the compatibility, especially regarding AES encryption.

From my understanding, the RC523 supports the ISO/IEC 14443 A protocol, which is also the standard for MUAES cards. However, I’ve read that the RC523 primarily supports Crypto1 encryption and doesn’t directly handle AES encryption.

I would like to clarify the following:

  1. Can the RC523 communicate with MUAES cards?
  2. If so, does the AES encryption need to be handled externally via an MCU or another security module?
  3. Are there any example codes or documentation available that could guide me through this implementation?

I would greatly appreciate any advice or guidance on this matter.

Thank you!

0 件の賞賛
返信
3 返答(返信)

1,042件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @jf555 

For MFRC523, there are not any examples. It's recommended that you can use CLRC663, and there is a dedicated example for MIFARE PLUS.

0 件の賞賛
返信

1,015件の閲覧回数
jf555
Contributor I
Hello, I understand that the CLRC663 is recommended for MIFARE Plus communication. Could you provide a specific example code or link regarding AES implementation to help with this?
0 件の賞賛
返信

999件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @jf555 

For CLRC663, you can download SW672315, there is an example for mifare plus, but which is security file, and need an NDA to get the download permission.

0 件の賞賛
返信