KW45 Change request for Datasheet about high RF input power during ISO testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW45 Change request for Datasheet about high RF input power during ISO testing

ソリューションへジャンプ
1,797件の閲覧回数
noriakimasuda
NXP Employee
NXP Employee

At KW45 datasheet, there is Max RF input power, Max +10dBm.

This is Max operational condition.

 

However, in case of ISO Testing, user need to apply +27dBm max (0.5W Max) of interfering wave with 5cm radiated.

It read about +14dBm @ RF input pin. It exceed the +10dBm.

 

Customer doesn't expect to work propearly up to +14dBm.

But they expects not to get damaged on IC by ISO testing.

 

So, Customer requests NXP to add the statement in datasheet like below.

“During ISO testing, by applying higher RF input power than +10dBm up to +20dBm, the device is still functional and not getting damaged”

This is just example of the wording, but could you discuss internally to add this kind of wording in datasheet at next document update?

 

0 件の賞賛
返信
1 解決策
1,722件の閲覧回数
noriakimasuda
NXP Employee
NXP Employee

Received feedback directly by e-mail

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,723件の閲覧回数
noriakimasuda
NXP Employee
NXP Employee

Received feedback directly by e-mail

0 件の賞賛
返信