KW45 Change request for Datasheet about high RF input power during ISO testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 Change request for Datasheet about high RF input power during ISO testing

Jump to solution
1,758 Views
noriakimasuda
NXP Employee
NXP Employee

At KW45 datasheet, there is Max RF input power, Max +10dBm.

This is Max operational condition.

 

However, in case of ISO Testing, user need to apply +27dBm max (0.5W Max) of interfering wave with 5cm radiated.

It read about +14dBm @ RF input pin. It exceed the +10dBm.

 

Customer doesn't expect to work propearly up to +14dBm.

But they expects not to get damaged on IC by ISO testing.

 

So, Customer requests NXP to add the statement in datasheet like below.

“During ISO testing, by applying higher RF input power than +10dBm up to +20dBm, the device is still functional and not getting damaged”

This is just example of the wording, but could you discuss internally to add this kind of wording in datasheet at next document update?

 

0 Kudos
Reply
1 Solution
1,683 Views
noriakimasuda
NXP Employee
NXP Employee

Received feedback directly by e-mail

View solution in original post

0 Kudos
Reply
1 Reply
1,684 Views
noriakimasuda
NXP Employee
NXP Employee

Received feedback directly by e-mail

0 Kudos
Reply