KW41Z with external amplifier

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW41Z with external amplifier

ソリューションへジャンプ
2,761件の閲覧回数
lukaszgesieniec
Contributor I

Where can I find software example how to use KW41Z with external amplifier? My application uses BLE and Thread.

I have to know how configure Wireless Connectivity stack to control RX_SWITCH and TX_SWITCH pads connected to my external amplifier.

I have connected external amp this way (fig from kw41z reference manual):

pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
1 解決策
2,543件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Lukasz,

To enable the TX/RX switch pins, you need to configure the mux of the pins, the timing registers for the TX/RX switch signals and enable the RX/TX_SWITCH on the FAD_CTRL register.

You can use the following code as reference. Include fsl_port.h and Phy.h.

    PORT_SetPinMux(PORTC,2u,kPORT_MuxAlt2); // PTC2 as TX_SWITCH
    PORT_SetPinMux(PORTC,3u,kPORT_MuxAlt2); // PTC3 as RX_SWITCH

    // TX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO2_TRIG_EN
    XCVR_TSM->TIMING49 = 0xFFFFFF01;

    // RX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO3_TRIG_EN
    XCVR_TSM->TIMING50 = 0xFF01FFFF;

    // Enable RX/TX_SWITCH
    PhyPlmeSetANTPadStateRequest(FALSE, TRUE);‍‍‍‍‍‍‍‍‍‍‍‍‍

Regards,

Gerardo

元の投稿で解決策を見る

2 返答(返信)
2,544件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Lukasz,

To enable the TX/RX switch pins, you need to configure the mux of the pins, the timing registers for the TX/RX switch signals and enable the RX/TX_SWITCH on the FAD_CTRL register.

You can use the following code as reference. Include fsl_port.h and Phy.h.

    PORT_SetPinMux(PORTC,2u,kPORT_MuxAlt2); // PTC2 as TX_SWITCH
    PORT_SetPinMux(PORTC,3u,kPORT_MuxAlt2); // PTC3 as RX_SWITCH

    // TX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO2_TRIG_EN
    XCVR_TSM->TIMING49 = 0xFFFFFF01;

    // RX_SWITCH output is derived from TSM output gpio2_trig_en
    // Timings for assertion/de-assertion for GPIO3_TRIG_EN
    XCVR_TSM->TIMING50 = 0xFF01FFFF;

    // Enable RX/TX_SWITCH
    PhyPlmeSetANTPadStateRequest(FALSE, TRUE);‍‍‍‍‍‍‍‍‍‍‍‍‍

Regards,

Gerardo

2,543件の閲覧回数
lukaszgesieniec
Contributor I

Thank you!

0 件の賞賛
返信