KW38A zephyr support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW38A zephyr support

Jump to solution
2,420 Views
cezarburlacu
Contributor I

Hello,

Are there any plans to port zephyr for NXP KW38 (frdm-kw38) or any hints where to start from? How different is from KW41z to use it as a template (Are there any application similar to AN12560)?

Any hint is highly appreciated.

Thanks

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,408 Views
nxf56274
NXP Employee
NXP Employee

Hi,

We do not have the plan to port zephyr to kw38. The zephyr has the porting guide.

We do not have the doc to describe the difference between kw41 and kw38.  

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,398 Views
cezarburlacu
Contributor I

Thank you for your response. It is a pity that zephyr is not supported for this board; it would've been the single one with BLE and CAN on the same chip...

0 Kudos
Reply
2,409 Views
nxf56274
NXP Employee
NXP Employee

Hi,

We do not have the plan to port zephyr to kw38. The zephyr has the porting guide.

We do not have the doc to describe the difference between kw41 and kw38.  

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply