KW36 filter for RSSI Ranging Application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36 filter for RSSI Ranging Application

ソリューションへジャンプ
4,793件の閲覧回数
Lincoln
Contributor III

Hi,

I want to filter RSSI value and I refer to the document below. In this section: 

Lincoln_Holmes_1-1631083937993.pngLincoln_Holmes_1-1631083937993.png

It suggests Gaussian combined with median filtering is relative stable(the last row in figure).

Is there any sample code available for Gaussian combined with median filtering? 

Thanks!

 

ラベル(2)
0 件の賞賛
返信
1 解決策
4,784件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Please refer the attachment.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,785件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Please refer the attachment.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信