KW36 filter for RSSI Ranging Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW36 filter for RSSI Ranging Application

Jump to solution
4,892 Views
Lincoln
Contributor III

Hi,

I want to filter RSSI value and I refer to the document below. In this section: 

Lincoln_Holmes_1-1631083937993.png

It suggests Gaussian combined with median filtering is relative stable(the last row in figure).

Is there any sample code available for Gaussian combined with median filtering? 

Thanks!

 

Labels (2)
0 Kudos
Reply
1 Solution
4,883 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Please refer the attachment.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
4,884 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Please refer the attachment.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply