KW36 can’t open Config Tools(Pin)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW36 can’t open Config Tools(Pin)

1,128 Views
danieltseng
Contributor V

The environment I use is as follows:

IDE:

 pastedImage_1.png

SDK:

 pastedImage_2.png

I want to use Pin config tool as follows:
Step1: Select project, then click "Open Pins"
pastedImage_3.png
Step2: The download progress bar of MKW36Z512xxx4 appears
pastedImage_5.png
Step 3: The message that does not support MKW36Z512xxx4 appears, as follows:
pastedImage_6.png
I have checked that my network is connected, and I still get an error signal.
How can I enter the pin Config Tool?
Labels (1)
0 Kudos
Reply
1 Reply

1,085 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Daniel Tseng

 

In the tab, ConfigTools->Data Manager make sure the FRDM-KW36 data is cached and up-to-date. Another suggestion I have is to download the latest SDK version, v2.2.3 Welcome | MCUXpresso SDK Builder 

 pastedImage_3.png

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos
Reply