KW36 can’t open Config Tools(Pin)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KW36 can’t open Config Tools(Pin)

1,492 次查看
danieltseng
Contributor V

The environment I use is as follows:

IDE:

 pastedImage_1.png

SDK:

 pastedImage_2.png

I want to use Pin config tool as follows:
Step1: Select project, then click "Open Pins"
pastedImage_3.png
Step2: The download progress bar of MKW36Z512xxx4 appears
pastedImage_5.png
Step 3: The message that does not support MKW36Z512xxx4 appears, as follows:
pastedImage_6.png
I have checked that my network is connected, and I still get an error signal.
How can I enter the pin Config Tool?
标签 (1)
0 项奖励
回复
1 回复

1,449 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Daniel Tseng

 

In the tab, ConfigTools->Data Manager make sure the FRDM-KW36 data is cached and up-to-date. Another suggestion I have is to download the latest SDK version, v2.2.3 Welcome | MCUXpresso SDK Builder 

 pastedImage_3.png

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 项奖励
回复