K32W baud rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W baud rate

2,487 Views
danieltseng
Contributor V

1. Update with "DK6 Production Flash Programmer".
    I know that when using LPC-Link2 USB connection can not reach 1M baud rate, what is the default speed?

    What is  the  highest speed that can be set in LPC-Link2?

2. If the SOC uses UART0 to connect to K32W,
    Can K32W receive 1M baud rate?

    Does RTS/CTS need to be connected?

Labels (1)
  • KW

0 Kudos
Reply
3 Replies

2,408 Views
danieltseng
Contributor V

I tried using "default baud rate"  and  "-P 115200", but it took about the same time for download.

"which speed are you referring  to"   on LPC-Link2 ?

 

0 Kudos
Reply

2,408 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Could you please try setting the verbosity in a higher level so we can verify about the boudrate ?

Regards,

Estephania

0 Kudos
Reply

2,408 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Do you mean with the SWD programming ? Or which speed are you referring  to ?

The questions 2 was already solved in https://community.nxp.com/thread/535671 

 

Regards,
Estephania

0 Kudos
Reply