K32W ISP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K32W ISP mode

2,517件の閲覧回数
danieltseng
Contributor V

If the SOC(Wifi module) is connected to K32W,

can Uart Rom Bootloader(ISP mode) run to 1M speed with no CTS/RTS ?

ラベル(1)
  • KW

0 件の賞賛
返信
3 返答(返信)

2,431件の閲覧回数
danieltseng
Contributor V

Thank you for your reply, let me know that 1M uart speed can be achieved without CTS/RTS.

0 件の賞賛
返信

2,431件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

it is good that this is clear now.

Regards,
Estephania

0 件の賞賛
返信

2,431件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

The device can support up to 1M speed , the usage of the CTS and RTS are mostly used in application level and is up to the customers if they use it or not.

In this case the flash programmer can work without CTS and RTS, you can check more information about this in the Production Flash Programmer Guide.

Regards,
Estephania

0 件の賞賛
返信