[JN5189] Unlock ISP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[JN5189] Unlock ISP mode

Jump to solution
3,422 Views
Johnny9
Contributor II

I am programming using DK6 programmer and jn5189's isp mode. I am locking the ISP using the " -w isp_level=" option, but I don't know how to unlock it. I did a search and it seems that there is a way to unlock the ISP using the "unlock key", but it is not explained well enough for me to understand, can someone explain it easily?

0 Kudos
Reply
1 Solution
3,381 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Johnny9

Hope you are doing well.

Please, refer to the file attached to this post, there you can find the script to create an unlock key and a document explaining ISP Access Levels and more information about the lock/unlock process.

Regards,
Eduardo.

View solution in original post

0 Kudos
Reply
3 Replies
3,295 Views
Johnny9
Contributor II

hello,


It's working fine as per your guide.
Thank you for your help.

I have an additional question,
What do 'Device ID', 'Max Device ID', 'Min Device ID' and 'Customer ID' mean and how do I use them in pFlash? They all default to '0'.

 

Regards,
Johnny9.

0 Kudos
Reply
3,382 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Johnny9

Hope you are doing well.

Please, refer to the file attached to this post, there you can find the script to create an unlock key and a document explaining ISP Access Levels and more information about the lock/unlock process.

Regards,
Eduardo.

0 Kudos
Reply
3,155 Views
seunghokims
Contributor III

Hello EduardoZamora

 

I have the same problem.

Please let us know which attachments you provided.

I would like to know how to unlock it.

Regards,

SeunhoKims.

 

 

0 Kudos
Reply