JN5189 I/O current capability?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JN5189 I/O current capability?

跳至解决方案
3,611 次查看
alnasl
Contributor I

Hi, I'm looking for the information about I/O current capability for the JN5189.

In the JN516x datasheet, there was a parameter called "Current sink/source capability" in the "I/O Characteristics" section, but there is no equivalent entry for the JN5189.

Usually, Cortex-M4 uCs have parameters like I_OH and I_OL (It's called "HIGH-level output current" and "LOW-level output current" in the LPC4000 series).

Am I missing something?

Thanks in advance!

标签 (1)
  • JN

0 项奖励
回复
1 解答
3,517 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @alnasl,

I truly apologize for the late response.

Could you please refer to JN5189 Data Sheet Section 13.3 IO Characteristics, Table 17 IO Characteristics? According to the expected load, then the VoL and VoH of the IOs are different.

For Low Speed IOs, max current should be 2mA per IO (IOs 0 to 9 and 12 to 16).
For High Speed IOs, max current should be 5mA per IO (IOs 17 to 21).
For IO with I2C, max current should be 2mA per IO.

EduardoZamora_2-1674237163621.png

EduardoZamora_3-1674237163624.png

Regards,
Eduardo.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,518 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @alnasl,

I truly apologize for the late response.

Could you please refer to JN5189 Data Sheet Section 13.3 IO Characteristics, Table 17 IO Characteristics? According to the expected load, then the VoL and VoH of the IOs are different.

For Low Speed IOs, max current should be 2mA per IO (IOs 0 to 9 and 12 to 16).
For High Speed IOs, max current should be 5mA per IO (IOs 17 to 21).
For IO with I2C, max current should be 2mA per IO.

EduardoZamora_2-1674237163621.png

EduardoZamora_3-1674237163624.png

Regards,
Eduardo.

0 项奖励
回复
3,498 次查看
alnasl
Contributor I

Thank you Eduardo.
I noticed that, but there’s no description about “maximum” current.
Can I take your answer as official information based on chip design?
Regards,

0 项奖励
回复
3,485 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Please consider these values as max for your design.

Regards,
Eduardo.

0 项奖励
回复
3,476 次查看
alnasl
Contributor I

Hello,

Thank you for your response.

I'll use these values for my design.

Regards,

0 项奖励
回复