JN5189 I/O current capability?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5189 I/O current capability?

Jump to solution
3,610 Views
alnasl
Contributor I

Hi, I'm looking for the information about I/O current capability for the JN5189.

In the JN516x datasheet, there was a parameter called "Current sink/source capability" in the "I/O Characteristics" section, but there is no equivalent entry for the JN5189.

Usually, Cortex-M4 uCs have parameters like I_OH and I_OL (It's called "HIGH-level output current" and "LOW-level output current" in the LPC4000 series).

Am I missing something?

Thanks in advance!

Labels (1)
  • JN

0 Kudos
Reply
1 Solution
3,516 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @alnasl,

I truly apologize for the late response.

Could you please refer to JN5189 Data Sheet Section 13.3 IO Characteristics, Table 17 IO Characteristics? According to the expected load, then the VoL and VoH of the IOs are different.

For Low Speed IOs, max current should be 2mA per IO (IOs 0 to 9 and 12 to 16).
For High Speed IOs, max current should be 5mA per IO (IOs 17 to 21).
For IO with I2C, max current should be 2mA per IO.

EduardoZamora_2-1674237163621.png

EduardoZamora_3-1674237163624.png

Regards,
Eduardo.

View solution in original post

0 Kudos
Reply
4 Replies
3,517 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @alnasl,

I truly apologize for the late response.

Could you please refer to JN5189 Data Sheet Section 13.3 IO Characteristics, Table 17 IO Characteristics? According to the expected load, then the VoL and VoH of the IOs are different.

For Low Speed IOs, max current should be 2mA per IO (IOs 0 to 9 and 12 to 16).
For High Speed IOs, max current should be 5mA per IO (IOs 17 to 21).
For IO with I2C, max current should be 2mA per IO.

EduardoZamora_2-1674237163621.png

EduardoZamora_3-1674237163624.png

Regards,
Eduardo.

0 Kudos
Reply
3,497 Views
alnasl
Contributor I

Thank you Eduardo.
I noticed that, but there’s no description about “maximum” current.
Can I take your answer as official information based on chip design?
Regards,

0 Kudos
Reply
3,484 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Please consider these values as max for your design.

Regards,
Eduardo.

0 Kudos
Reply
3,475 Views
alnasl
Contributor I

Hello,

Thank you for your response.

I'll use these values for my design.

Regards,

0 Kudos
Reply