JN5189 Config memory restoring

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5189 Config memory restoring

5,808 Views
Marcin1
Contributor II

Hello,

For reasons that I will wirte about in another post, I erased Config memory on JN5189 using DK6Programmer and now I cannot communicate with with device using DK6Programmer

I would like to ask for way to restore this memory, please.

 

Marcin

Labels (1)
  • JN

0 Kudos
Reply
10 Replies

5,792 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

What is the command that you used to erase that specific memory?

The JN5189 provides a bootloader in ROM that could help you with this setup.

What is the command that you are typing?

Could you please type the next command?

DK6Programmer.exe -s COM11 -h

mario_castaneda_0-1638312965771.png

Regards,

Mario

0 Kudos
Reply

5,784 Views
Marcin1
Contributor II

Hi @mario_castaneda ,

Thank you for fast response.

I used command:

DK6Programmer.exe -s COM11 -e Config

Every command with DK6Programmer.exe -s COMx for chip with erased Config memory i got:

Error opening connection: Read error

Response after -h command:

Error po erase Config memory.png

 

 

Regards,

Marcin

0 Kudos
Reply

5,751 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

Could you please try to press the ISP button before you type the command?

However, is it possible that you could try to program the device using the MCUxpresso using CMSIS or Jink?

Regards,

Mario

 

 

0 Kudos
Reply

5,721 Views
Marcin1
Contributor II

Hi, @mario_castaneda 

I can not program my device using MCUxpresso.

Sorry but it is also not that simple to press ISP button in my system.

Is there any other options to fix it?

If not I will try to press ISP button but it makes me to put a lot of effort.

Regards,

Marcin

 

5,647 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

Did you get the previous Config information?

DK6Programmer.exe -s COM11 -r Config

some parameters (trimming parameter) are written in our factory, they would necessarily be different so you could expect problems in the radio behavior if we write different ones.

Please do not erase the Config information.

Regards,

Mario

0 Kudos
Reply

5,634 Views
Marcin1
Contributor II

Hi @mario_castaneda ,

Thank you for your response.

I'm sorry, but I can not get previous Config information from that chip. I can get it from other chip if it's needed.

The problem is that -s function does not work for that chip.

Is there any other option to write data besides DK6Programmer -s COMx function?

Regards,

Marcin

0 Kudos
Reply

5,620 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

Please do not erase the config file.

I highly suggest that must not erase the CONFIG page, and for the erased device, if you do not save the previous information the device is can not be recovered because it needs some parameters from our factory.

What config values that you want to modify?

Regards,

Mario

0 Kudos
Reply

5,541 Views
Marcin1
Contributor II

Hi @mario_castaneda 

I would like to know if there is way to somehow write new config values into Config memory.

I do not know which values i need to modify. I suppose that I need to write all of them.

Regards,

Marcin

0 Kudos
Reply

5,531 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Marcin,

I look if there is a way to reprogram the CONFIG values.

I highly suggest you that must not erase the CONFIG page.

Unfortunately, the erased device is bricked. Each device has different CONFIG values preprogrammed in our manufacture.

Sorry for any inconvenience that this may cause you.

Regards,

Mario

5,668 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Marcin1,

I am checking the problem that you have. The command erases the complete config information and the tool needs that information for programming purpose.

I am checking if there is a way that you could reprogram some values in this case.

Please do not type this command again.

Regards,

Mario