JN5179

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5179

2,410件の閲覧回数
wupengfei
Contributor II

To put the module into UART programming mode, tie MISO to 0 V while releasing
RESET. This causes the device to read zeros back from the Flash memory during
initialization and, as a result, to enter programming mode. If you are using the module in
conjunction with a serial interface then the signal PGM is available to put the device into
programming mode. To allow this signal to operate correctly from the Flash programming
software.

What is the signal PGM?

0 件の賞賛
返信
1 返信

2,094件の閲覧回数
davidashraf
Contributor V

wupengfei‌ 

I believe that's is the way to enter programming mode 
https://community.nxp.com/thread/460072 

0 件の賞賛
返信