JN5179

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5179

2,430 Views
wupengfei
Contributor II

To put the module into UART programming mode, tie MISO to 0 V while releasing
RESET. This causes the device to read zeros back from the Flash memory during
initialization and, as a result, to enter programming mode. If you are using the module in
conjunction with a serial interface then the signal PGM is available to put the device into
programming mode. To allow this signal to operate correctly from the Flash programming
software.

What is the signal PGM?

0 Kudos
Reply
1 Reply

2,114 Views
davidashraf
Contributor V

wupengfei‌ 

I believe that's is the way to enter programming mode 
https://community.nxp.com/thread/460072 

0 Kudos
Reply